Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28377D-EP: Inquiries regarding the Flash API

Part Number: TMS320F28377D-EP

We are currently developing a system using the TMS320F28377D-EP.
We need to use either `F021_API_F2837xD_FPU32_EABI.lib` or `F021_API_F2837xD_FPU32.lib` to store user data in a specific region of the internal Flash.
The issue is that we are required to conduct reliability testing, but verification is not possible using only the library files. Could you provide the source code for these library files?

  • Hi Lee,

    TI can provide the source code for these library files under NDA. Even then, the source is for review and audit only. Your application must still link the TI-supplied .lib, unmodified and not rebuilt. TI does not allow recompiling of the code.

    Regards 
    Arpit