Part Number: TMS320F28054M
Hi,
I am seeing motor vibrations every 6.6s when the motor is standing still using the TMS320F28054M microcontroller. What can I change in user.h to resolve this issue? Or is this a deeper control loop issue?
Thanks,
GB
Part Number: TMS320F28054M
Hi,
I am seeing motor vibrations every 6.6s when the motor is standing still using the TMS320F28054M microcontroller. What can I change in user.h to resolve this issue? Or is this a deeper control loop issue?
Thanks,
GB
Hi GB,
Are you using any TI EVM? What is your motor parameters?
Thanks,
Jiaxin
Hi Jiaxin,
These are my motor parameters:
#define USER_MOTOR_TYPE MOTOR_Type_Pm #define USER_MOTOR_NUM_POLE_PAIRS (2) #define USER_MOTOR_Rr (NULL) #define USER_MOTOR_Rs (1.892402) #define USER_MOTOR_Ls_d (0.00023) #define USER_MOTOR_Ls_q (0.00023) #define USER_MOTOR_RATED_FLUX (0.0835702) #define USER_MOTOR_MAGNETIZING_CURRENT (NULL) #define USER_MOTOR_RES_EST_CURRENT (1.5) #define USER_MOTOR_IND_EST_CURRENT (-1.5) #define USER_MOTOR_MAX_CURRENT (6.5) #define USER_MOTOR_FLUX_EST_FREQ_Hz (60.0)//100 #define USER_MOTOR_ENCODER_LINES (1024.0) #define USER_MOTOR_MAX_SPEED_KRPM (5.6) #define USER_SYSTEM_INERTIA (0.01061397791) #define USER_SYSTEM_FRICTION (0.01320964098)
Thanks,
GB