Hi
I want to connect a 3-phase motor to mi renevable energy kit, so I have to do the set up for the inverter, with the 3 phases.
In the example, provided by Texas, only 2 phases works, and there is my problem: When I enable the third phase, an error happens:
Error:
Error 0xA0001020/-1062
Error during: Execution, Target,
Device driver: Power Loss Detected on Target CPU.
This could also result from disconnecting the emulator from the target.
It is recommended to RESET EMULATOR. This will disconnect each
target from the emulator. The targets should then be power cycled
or hard reset followed by an emureset and reconnect to each target.
I work with Simulink, and, if I only use 2 of the 3 phases, everything goes ok.
If someone knows how sholud I do the set up (written in C or in Simulink, whatever),please, help me, because I can´t find any example of this. And also I can´t find the possible source of the problem
Thanks in advanced!
P.D. I work on TMS320C2000 with 25038 and CC 3.3 in XP, connected with JTAG (XDS510LCusb) , with Matlab 2011a