Part Number: F29H850TU
Other Parts Discussed in Thread: XDS110ISO-EVM, F29H85X-SOM-EVM, SYSCONFIG
Hi,
My customer is about to set up the development environment for F29H85X-SOM-EVM + XDS110ISO-EVM, but we are uncertain which specific versions of SDK, CCS, CGT and SysConfig should be installed.
Should the latest versions of these tools be installed ?
Based on my previous experiences, mismatches between the versions of SDK, CCS have led to some errors, so I’m concerned about using the latest versions without verification.
Could you please recommend a stable combination of versions for these tools setup ?
The latest version of each tool as follows;
F29x Motor Control SDK 1.00.00.00
F29H85x SDK 26.01.00 LTS
CCS 21.0.1
C29-CGT 2.2.2 LTS
SysConfig 1.28.1.4785
However, Mortor Control SDK supports F29 SDK 1.00.00.00. The Getting Started of Motor Control SDK jumps to the Getting Started of F29H85x-SDK 1.00.00.00.
Which combination as follows do you recommend ? It depends on F29H85x SDK 1.00.00.00 or 26.01.00 LTS.
- F29x Motor Control SDK 1.00.00.00
- F29H85x SDK 1.00.00.00
According to the release note of F29H85x-SDK 1.00.00.00, the dependencies are
CCS 20.0.0
C29 CGT 1.0.0.LTS
SysConfig 1.25
Python v3.X
OpenSSL v3.X.X
- F29x Motor Control SDK 1.00.00.00
- F29H85x SDK 26.01.00 LTS
According to the release note of F29H85x-SDK 26.01.00, the dependencies are
CCS 21.0.1
C29 CGT 2.2.1.LTS
SysConfig 1.28.1
Python v3.X
OpenSSL v3.X.X
Thanks and regards,
Hideaki