Part Number: UNIFLASH
ARM Linux is now the common host platform for embedded production and test equipment. Raspberry Pi-class boards, NVIDIA Jetson modules, and custom Linux carrier boards drive today’s manufacturing fixtures, field service tools, and programming stations. UniFlash currently supports only x86_64 Linux, Windows, and macOS, so none of these can run it.
This matters most in volume production. Contract manufacturers and OEMs want flashing stations that are low-cost, low-power, and fanless. Where the rest of a line is ARM-based, UniFlash forces an extra x86 machine whose only job is to run one tool. That adds cost, power draw, and a separate system to maintain, and it falls on customers who have already chosen TI silicon.
A phased approach could keep the effort modest. UniFlash’s command-line engine (dslite) is already a separate entry point from the GUI, so a headless aarch64 build covering scriptable JTAG and UART flashing would serve most production needs. The GUI could follow later or not at all.
The benefit is that AM26x customers can scale production flashing on the infrastructure they already run, and TI removes an adoption barrier for its MCU families in automated manufacturing.