TMS320F28P650DK: SPI Communication with FRAM

Part Number: TMS320F28P650DK

We are using FRAM FM25W256-G with TMS320f28p65x and communicating via SPI. FRAM recommends using Mode 0 for communication, but when I set this and SPI communication doesn't work, but it works when I set Mode 1 configurtion in controller.

After going through some documents, we found that the mode 0 standard and mode 0 of TI doesn't work the same w.r.t to clock and COPI or CIPO timings.

So, after further sturdy we can see the timing diagram of Mode 0 standard (CPOL = 0, CPHA = 0) is similar to controller spi mode 1 settings(CLKPOLARITY = 0, CLK_PHASE = 1).

So, we wanted to reconfirm if this is correct and why in none of the documents it is mentioned about this inverse relation?