Part Number: TMS320F2800157-Q1
I am using TI’s TMS320F2800157-Q1 and implementing a LIN slave task using the SCI module, which is configured to use its FIFO.
Upon receiving a Break Field, a framing error is detected; I then execute `SCI_performSoftwareReset` to clear this error.
However, when the subsequent Sync Field arrives, the low-level signal from the Break Field is incorrectly interpreted as the start bit of the Sync Field.
What steps should I take to ensure that the next falling edge is correctly recognized as the start bit of the Sync Field?