Other Parts Discussed in Thread: TMS320F28335, TMS320C28346, ADS62P25
Are there any equivalent MCUs for the TMS320C28346 and/or TMS320F28335 in the ARM series?
I am attempting to interface with the following in as near real time as possible:
Sample an ADS62P25 at as near full speed as possible
Output 24 Bits of data to a 480X272 TFT LCD at 9.2MHz
The following will also need to be interfaced with but on an as needed basis:
Store sampled values to FLASH memory via SPI
Control frequency output of Clock Generator (initial configuration at startup)
Control frequency output of Waveform generator (Analog AD9853) via SPI
Control amplitude of waveform generator by digital potentiometer (Maxim MAX5481) via SPI
Configure ADS62P25 via SPI
Control Scaling and Coupling of Analog Front End (Solid State Relays and 2:4 Multiplexers)
Sample battery voltage
Please note, inorder to get multiple SPI devices on one bus, I am utilizing a 1:8 Multiplexer as well for the chip select.