This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Incompatible version detected. DSP/BIOS version does not satisfy product requirements!

Hi

Iam using f28035 kit . Iam using 2011b matlab and CCS V4.

when i build the simulink model, I always get the following error message:

The call to idelink_ert_make_rtw_hook, during the exit hook generated the following error:
Error while loading and running the project.

The build process will terminate as a result.
and,
when i typed at the MATLAB prompt ampquot;checkEnvSetup(‘ccs’,'f28035′)ampquot;, i got the following incompitability errors of CCS v3.3 as depicted below:
ampgt;ampgt; checkEnvSetup(‘ccs’,'f28035′)
1. Checking CCS (Code Composer Studio) version
Required version: 3.3.82.13
Required by : Embedded IDE Link 4.1
Required for : Automation and Code Generation
Your Version : 3.3.83.19
 Incompatible version detected. CCS version does not satisfy product requirements!
2. Checking CGT (Texas Instruments C2000 Code Generation Tools) version
   Required version: 5.2.1
   Required by     : Embedded IDE Link 4.1
   Required for    : Code generation
Warning: Illegal right hand side in assignment. Too many elements.
> In C:\Program Files\MATLAB\R2010a\toolbox\idelink\extensions\ticcs\envChecker\checkEnvSetup_private.p>envSetup at 285
  In C:\Program Files\MATLAB\R2010a\toolbox\idelink\extensions\ticcs\envChecker\checkEnvSetup_private.p>checkEnvSetup_private at 68
  In checkEnvSetup at 131
   Your Version    :
   Incompatible version detected. CGT version does not satisfy product requirements!
3. Checking DSP/BIOS (Real Time Operating System) version
   Required version: 5.33.05
   Required by     : Embedded IDE Link 4.1
   Required for    : Real-Time Data Exchange (RTDX)
Warning: Illegal right hand side in assignment. Too many elements.
> In C:\Program Files\MATLAB\R2010a\toolbox\idelink\extensions\ticcs\envChecker\checkEnvSetup_private.p>envSetup at 285
  In C:\Program Files\MATLAB\R2010a\toolbox\idelink\extensions\ticcs\envChecker\checkEnvSetup_private.p>checkEnvSetup_private at 68
  In checkEnvSetup at 131
   Your Version    :
   Incompatible version detected. DSP/BIOS version does not satisfy product requirements!

i cant find this directory $(DSP2802x_INSTALLDIR)

Matlab could nt find the header , and flash API's  utility files   pls help in this regard.

Previously I was used f28335 it is generating code and interface with the ccs v4. when iam going to use f28035 im getting problem .

krishnaveni