hi to all,
I am working with F28335 device with CCS Version: 4.2.1.00004 .for this i want to calculate the Check sum for my application ,is there any special mechanism to calculate the check sum ,if so where the checksum will store .....
> I am following the Addition of the consecutive bytes/words if it is a write mechanism for this ,where i should store the check Sum.
> basically we will store the checksum in last location of the flash.But this device will have CSM area in that location
can any one help me on this issue
thanks in Advance