Other Parts Discussed in Thread: TMS320F28335
I'm trying to connect an EVAL-AD2S1210 resolver to digital board to an eZdsp which has a TMS320F28335. I want to connect the two boards using the EVAL-AD2S1210's parallel port, but I'm not sure what connections to use on the eZdsp. The parallel port on the EVAL-AD2S1210 is a 26 way connector.
Has anyone ever made this type of connection before? Would anyone know how to do this type of interfacing?
I'm thinking that I need to use the expansion ports on the eZdsp in some way - possibly the P10, P2 or P8 expansions?