Other Parts Discussed in Thread: CONTROLSUITE
Hello,
I am trying to spin a 3-ph BLDC motor using a 28035 processor and snsorless field oriented control. The specs for the motor are as follows:
- RS = 0.126 ohm
- LS = 0.000125 H
- # of poles = 4
- Voltage = 9-18V (12V nominal)
- Current = 4.1A at rated speed of 3300RPM
- Motor Driver / Phase Inverter that is being used to drive the motor phases = Faichild FSBF10CH60B
I've been using the sensorless FOC of 3-ph PMSM based examples to drive the motor but am having issues in properly tuning the SMO and speed PID using the different parameters in order to get the motor above to run reliably. I was able to find a DMClib Condfiguration spreadhsheet under ControlSuite in the following folder C:\TI\controlSUITE\libs\app_libs\motor_control\math_blocks\v3.1
Is there an app note or any documentation that explains how to use this spreadsheet?
Any help would be greatly appreciated.
Thank you
Terry