This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Concerto - M3 WatchDog

Guru 10750 points


Hi,

I'm trying to run the WD example under MWare_v120\F28M35x_examples_Master\watchdog\m3 but I never gets to the WD interrupt "WatchdogTimerHandler" why is that?

Thanks,

HR

  • I am facing same problem. Not getting interrupt of watchdog. Due to that my system is resetting at (2*watchdog set time).


    /*****************************************************/
    ////************WATCHDOG FUNCTION *****************////
    // watch dog 0 has clock source as system clock
    // watchdog1 has clock source as oscl clock
    SysCtlPeripheralEnable(SYSCTL_PERIPH_WDOG0); //Watch dog enable for Hang Issue

    // watchdog counter reset
    WatchdogReloadSet(WATCHDOG0_BASE, 375000);// Reload of watchdog with 20000000 * 6.6667 * 2ns = 266ms
    //
    WatchdogUnlock(WATCHDOG0_BASE);
    // Enable watchdog reset generation
    WatchdogResetEnable(WATCHDOG0_BASE);
    IntRegister(WATCHDOG0_BASE, WatchdogTimerHandler);
    IntEnable(INT_WATCHDOG);// Enable Interrupt of watchdog
    // Enable watchdog
    WatchdogEnable(WATCHDOG0_BASE);
    // Lock the Watchdog0
    WatchdogLock(WATCHDOG0_BASE);
    //Interrupt registration for watchdog



    @125us, I am resetting it,

    if(Mcore.adj.SPARE0121 == 5){
    FRAM3_EN;
    }
    else{
    WatchdogUnlock(WATCHDOG0_BASE);
    WatchdogReloadSet(WATCHDOG0_BASE, 375000);
    WatchdogLock(WATCHDOG0_BASE);
    }
    when i set spare0121 = 5, it should go in watchdog interrupt.


    @ISR

    void WatchdogTimerHandler (void)
    {
    CounterWD++;
    FRAM3_DIS;
    WatchdogIntClear(WATCHDOG0_BASE);

    }




    My counter is not incrementing.
    and GPIO -> FRAM 3is not changing when it comes in interrupt.


    Umang