Other Parts Discussed in Thread: TMS320F28335
I have a simple application that runs out of flash on a TMS320F28335.The application runs fine when executed from the debugger/emulator environment.
However after I reset the power, the device does not boot up the application correctly.
I.e. It runs out of flash when executed from the debugger, but not after a power reset.
I have run other sample applications from flash after a reboot and they run just fine. I've tried comparing the project settings and they look the same as my application.
What special considerations do I need to make (project settings) to allow my application to run after a power reset?
I have code composer studio CCS v5 and USB2000 Emulator.
thanks in advance,
Paul