Hi ,

                previously i discussed with you all about f2812 SCI Boot mode, please finally answer  one more question.

1. what linker file i have to add to compile the source code for SCI BOOT Mode HEX FILE ?

I HAVE TWO LINKER FILES , I ATTACHED WITH THIS MAIL, PLEASE CORRECT AND SENT IT TO ME , ...

I HAVE TO FINISH MY PROJECT AS SOON.........., PLEASE HELP ME

/*
// TI File $Revision: /main/2 $
// Checkin $Date: April 28, 2005   15:19:56 $
//###########################################################################
//
// FILE:	F2812.cmd
//
// TITLE:	Linker Command File For F2812 Device
//
//###########################################################################
// $TI Release: DSP281x C/C++ Header Files V1.20 $
// $Release Date: July 27, 2009 $
//###########################################################################
*/

/* ======================================================
// For Code Composer Studio V2.2 and later
// ---------------------------------------
// In addition to this memory linker command file, 
// add the header linker command file directly to the project. 
// The header linker command file is required to link the
// peripheral structures to the proper locations within 
// the memory map.
//
// The header linker files are found in <base>\DSP281x_Headers\cmd
//   
// For BIOS applications add:      DSP281x_Headers_nonBIOS.cmd
// For nonBIOS applications add:   DSP281x_Headers_nonBIOS.cmd    
========================================================= */

/* ======================================================
// For Code Composer Studio prior to V2.2
// --------------------------------------
// 1) Use one of the following -l statements to include the 
// header linker command file in the project. The header linker
// file is required to link the peripheral structures to the proper 
// locations within the memory map                                    */

/* Uncomment this line to include file only for non-BIOS applications */
/* -l DSP281x_Headers_nonBIOS.cmd */

/* Uncomment this line to include file only for BIOS applications */
/* -l DSP281x_Headers_BIOS.cmd */

/* 2) In your project add the path to <base>\DSP281x_headers\cmd to the
   library search path under project->build options, linker tab, 
   library search path (-i).
/*========================================================= */

/* Define the memory block start/length for the F2812  
   PAGE 0 will be used to organize program sections
   PAGE 1 will be used to organize data sections

   Notes: 
         Memory blocks on F2812 are uniform (ie same
         physical memory) in both PAGE 0 and PAGE 1.  
         That is the same memory region should not be
         defined for both PAGE 0 and PAGE 1.
         Doing so will result in corruption of program 
         and/or data. 
*/

MEMORY
{
PAGE 0:    /* Program Memory */
           /* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE1 for data allocation */

   ZONE0       : origin = 0x002000, length = 0x002000     /* XINTF zone 0 */
   ZONE1       : origin = 0x004000, length = 0x002000     /* XINTF zone 1 */
   RAML0       : origin = 0x008000, length = 0x001000     /* on-chip RAM block L0 */
   ZONE2       : origin = 0x080000, length = 0x080000     /* XINTF zone 2 */
   ZONE6       : origin = 0x100000, length = 0x080000     /* XINTF zone 6 */
   OTP         : origin = 0x3D7800, length = 0x000800     /* on-chip OTP */
   FLASHJ      : origin = 0x3D8000, length = 0x002000     /* on-chip FLASH */
   FLASHI      : origin = 0x3DA000, length = 0x002000     /* on-chip FLASH */
   FLASHH      : origin = 0x3DC000, length = 0x004000     /* on-chip FLASH */
   FLASHG      : origin = 0x3E0000, length = 0x004000     /* on-chip FLASH */
   FLASHF      : origin = 0x3E4000, length = 0x004000     /* on-chip FLASH */
   FLASHE      : origin = 0x3E8000, length = 0x004000     /* on-chip FLASH */
   FLASHD      : origin = 0x3EC000, length = 0x004000     /* on-chip FLASH */
   FLASHC      : origin = 0x3F0000, length = 0x004000     /* on-chip FLASH */
   FLASHA      : origin = 0x3F6000, length = 0x001F80     /* on-chip FLASH */
   CSM_RSVD    : origin = 0x3F7F80, length = 0x000076     /* Part of FLASHA.  Program with all 0x0000 when CSM is in use. */
   BEGIN       : origin = 0x3F7FF6, length = 0x000002     /* Part of FLASHA.  Used for "boot to Flash" bootloader mode. */
   CSM_PWL     : origin = 0x3F7FF8, length = 0x000008     /* Part of FLASHA.  CSM password locations in FLASHA */
   
/* ZONE7       : origin = 0x3FC000, length = 0x003FC0     /* XINTF zone 7 available if MP/MCn=1 */ 
   ROM         : origin = 0x3FF000, length = 0x000FC0     /* Boot ROM available if MP/MCn=0 */
   RESET       : origin = 0x3FFFC0, length = 0x000002     /* part of boot ROM (MP/MCn=0) or XINTF zone 7 (MP/MCn=1) */
   VECTORS     : origin = 0x3FFFC2, length = 0x00003E     /* part of boot ROM (MP/MCn=0) or XINTF zone 7 (MP/MCn=1) */

PAGE 1 :   /* Data Memory */
           /* Memory (RAM/FLASH/OTP) blocks can be moved to PAGE0 for program allocation */
           /* Registers remain on PAGE1                                                  */

   RAMM0       : origin = 0x000000, length = 0x000400     /* on-chip RAM block M0 */
   RAMM1       : origin = 0x000400, length = 0x000400     /* on-chip RAM block M1 */
   RAML1       : origin = 0x009000, length = 0x001000     /* on-chip RAM block L1 */
   FLASHB      : origin = 0x3F4000, length = 0x002000     /* on-chip FLASH */
   RAMH0       : origin = 0x3F8000, length = 0x002000     /* on-chip RAM block H0 */
}

/* Allocate sections to memory blocks.
   Note:
         codestart user defined section in DSP28_CodeStartBranch.asm used to redirect code 
                   execution when booting to flash
         ramfuncs  user defined section to store functions that will be copied from Flash into RAM
*/ 
 
SECTIONS
{
 
   /* Allocate program areas: */
   .cinit              : > FLASHA      PAGE = 0
   .pinit              : > FLASHA,     PAGE = 0
   .text               : > FLASHA      PAGE = 0
   codestart           : > BEGIN       PAGE = 0
   ramfuncs            : LOAD = FLASHD, 
                         RUN = RAML0, 
                         LOAD_START(_RamfuncsLoadStart),
                         LOAD_END(_RamfuncsLoadEnd),
                         RUN_START(_RamfuncsRunStart),
                         PAGE = 0

   csmpasswds          : > CSM_PWL     PAGE = 0
   csm_rsvd            : > CSM_RSVD    PAGE = 0
   
   /* Allocate uninitalized data sections: */
   .stack              : > RAMM0       PAGE = 1
   .ebss               : > RAML1       PAGE = 1
   .esysmem            : > RAMH0       PAGE = 1

   /* Initalized sections go in Flash */
   /* For SDFlash to program these, they must be allocated to page 0 */
   .econst             : > FLASHA      PAGE = 0
   .switch             : > FLASHA      PAGE = 0      

   /* Allocate IQ math areas: */
   IQmath              : > FLASHC      PAGE = 0                  /* Math Code */
   IQmathTables        : > ROM         PAGE = 0, TYPE = NOLOAD   /* Math Tables In ROM */

   /* .reset is a standard section used by the compiler.  It contains the */ 
   /* the address of the start of _c_int00 for C Code.   /*
   /* When using the boot ROM this section and the CPU vector */
   /* table is not needed.  Thus the default type is set here to  */
   /* DSECT  */ 
   .reset              : > RESET,      PAGE = 0, TYPE = DSECT
   vectors             : > VECTORS     PAGE = 0, TYPE = DSECT

}
.....,

/*
// TI File $Revision: /main/4 $
// Checkin $Date: July 9, 2009   17:39:29 $
//###########################################################################
//
// FILE:    DSP281x_Headers_nonBIOS.cmd
//
// TITLE:   DSP281x Peripheral registers linker command file 
//
// DESCRIPTION: 
// 
//          This file is for use in Non-BIOS applications.
//
//          Linker command file to place the peripheral structures 
//          used within the DSP28 headerfiles into the correct memory
//          mapped locations.
//
//          This version of the file includes the PieVectorTable structure.
//          For BIOS applications, please use the DSP281x_Headers_BIOS.cmd file
//          which does not include the PieVectorTable structure.
//
//###########################################################################
// $TI Release: DSP281x C/C++ Header Files V1.20 $
// $Release Date: July 27, 2009 $
//###########################################################################
*/

MEMORY
{
 PAGE 0:    /* Program Memory */

 PAGE 1:    /* Data Memory */
 
   DEV_EMU     : origin = 0x000880, length = 0x000180     /* device emulation registers */
   PIE_VECT    : origin = 0x000D00, length = 0x000100     /* PIE Vector Table */
   FLASH_REGS  : origin = 0x000A80, length = 0x000060     /* FLASH registers */
   CSM         : origin = 0x000AE0, length = 0x000010     /* code security module registers */
   XINTF       : origin = 0x000B20, length = 0x000020     /* external interface registers */
   CPU_TIMER0  : origin = 0x000C00, length = 0x000008     /* CPU Timer0 registers */
   CPU_TIMER1  : origin = 0x000C08, length = 0x000008     /* CPU Timer1 registers */
   CPU_TIMER2  : origin = 0x000C10, length = 0x000008     /* CPU Timer2 registers */
   PIE_CTRL    : origin = 0x000CE0, length = 0x000020     /* PIE control registers */
   ECANA       : origin = 0x006000, length = 0x000040     /* eCAN control and status registers */ 
   ECANA_LAM   : origin = 0x006040, length = 0x000040     /* eCAN local acceptance masks */
   ECANA_MOTS  : origin = 0x006080, length = 0x000040     /* eCAN message object time stamps */
   ECANA_MOTO  : origin = 0x0060C0, length = 0x000040     /* eCAN object time-out registers */
   ECANA_MBOX  : origin = 0x006100, length = 0x000100     /* eCAN mailboxes */
   SYSTEM      : origin = 0x007010, length = 0x000020     /* System control registers */
   SPIA        : origin = 0x007040, length = 0x000010     /* SPI registers */
   SCIA        : origin = 0x007050, length = 0x000010     /* SCI-A registers */
   XINTRUPT    : origin = 0x007070, length = 0x000010     /* external interrupt registers */
   GPIOMUX     : origin = 0x0070C0, length = 0x000020     /* GPIO mux registers */
   GPIODAT     : origin = 0x0070E0, length = 0x000020     /* GPIO data registers */
   ADC         : origin = 0x007100, length = 0x000020     /* ADC registers */
   EVA         : origin = 0x007400, length = 0x000040     /* Event Manager A registers */
   EVB         : origin = 0x007500, length = 0x000040     /* Event Manager B registers */
   SCIB        : origin = 0x007750, length = 0x000010     /* SCI-B registers */
   MCBSPA      : origin = 0x007800, length = 0x000040     /* McBSP registers */
   CSM_PWL     : origin = 0x3F7FF8, length = 0x000008     /* Part of FLASHA.  CSM password locations. */
}

 
SECTIONS
{
   PieVectTableFile : > PIE_VECT,   PAGE = 1

/*** Peripheral Frame 0 Register Structures ***/
   DevEmuRegsFile    : > DEV_EMU,     PAGE = 1
   FlashRegsFile     : > FLASH_REGS,  PAGE = 1
   CsmRegsFile       : > CSM,         PAGE = 1
   XintfRegsFile     : > XINTF,       PAGE = 1
   CpuTimer0RegsFile : > CPU_TIMER0,  PAGE = 1 
   CpuTimer1RegsFile : > CPU_TIMER1,  PAGE = 1 
   CpuTimer2RegsFile : > CPU_TIMER2,  PAGE = 1  
   PieCtrlRegsFile   : > PIE_CTRL,    PAGE = 1      

/*** Peripheral Frame 1 Register Structures ***/
   ECanaRegsFile     : > ECANA,       PAGE = 1
   ECanaLAMRegsFile  : > ECANA_LAM    PAGE = 1   
   ECanaMboxesFile   : > ECANA_MBOX   PAGE = 1
   ECanaMOTSRegsFile : > ECANA_MOTS   PAGE = 1
   ECanaMOTORegsFile : > ECANA_MOTO   PAGE = 1

/*** Peripheral Frame 2 Register Structures ***/
   SysCtrlRegsFile   : > SYSTEM,      PAGE = 1
   SpiaRegsFile      : > SPIA,        PAGE = 1
   SciaRegsFile      : > SCIA,        PAGE = 1
   XIntruptRegsFile  : > XINTRUPT,    PAGE = 1
   GpioMuxRegsFile   : > GPIOMUX,     PAGE = 1
   GpioDataRegsFile  : > GPIODAT      PAGE = 1
   AdcRegsFile       : > ADC,         PAGE = 1
   EvaRegsFile       : > EVA,         PAGE = 1
   EvbRegsFile       : > EVB,         PAGE = 1
   ScibRegsFile      : > SCIB,        PAGE = 1
   McbspaRegsFile    : > MCBSPA,      PAGE = 1
   
/*** Code Security Module Register Structures ***/
   CsmPwlFile        : > CSM_PWL,     PAGE = 1
}


/******************* end of file ************************/



MEMORY
{
PAGE 0 :
   /* For this example, H0 is split between PAGE 0 and PAGE 1 */  
   /* BEGIN is used for the "boot to HO" bootloader mode      */
   /* RESET is loaded with the reset vector only if           */
   /* the boot is from XINTF Zone 7.  Otherwise reset vector  */
   /* is fetched from boot ROM. See .reset section below      */
   
   RAMM0      : origin = 0x000000, length = 0x000400
   BEGIN      : origin = 0x3F8000, length = 0x000002             
   PRAMH0     : origin = 0x3F8002, length = 0x000FFE
   RESET      : origin = 0x3FFFC0, length = 0x000002           

         
PAGE 1 : 

   /* For this example, H0 is split between PAGE 0 and PAGE 1 */

   RAMM1    : origin = 0x000400, length = 0x000400
   DRAMH0   : origin = 0x3f9000, length = 0x001000         
}
 
 
SECTIONS
{
   /* Setup for "boot to H0" mode: 
      The codestart section (found in DSP28_CodeStartBranch.asm)
      re-directs execution to the start of user code.  
      Place this section at the start of H0  */

   codestart        : > BEGIN,       PAGE = 0
   ramfuncs         : > PRAMH0       PAGE = 0  
   .text            : > PRAMH0,      PAGE = 0
   .cinit           : > PRAMH0,      PAGE = 0
   .pinit           : > PRAMH0,      PAGE = 0
   .switch          : > RAMM0,       PAGE = 0
   .reset           : > RESET,       PAGE = 0, TYPE = DSECT /* not used, */
   
   .stack           : > RAMM1,       PAGE = 1
   .ebss            : > DRAMH0,      PAGE = 1
   .econst          : > DRAMH0,      PAGE = 1      
   .esysmem         : > DRAMH0,      PAGE = 1

     
}

Many Thanks,

Thiyagarajan.S