Hi There
Is it possible to use a GPIO pin for something else if the EPWM that is mux'd to that pin is being used as an ADC trigger? i.e. should the pin be reserved?
Ta
(F28027 controlSTICK)
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Toby,
Yes. You can run the PWM internally without using the Output. Just make sure you have the GPIO MUX set to GPIO and not PWM.
Regards,
Daniel