Other Parts Discussed in Thread: TMS320LF2406A, CODECOMPOSER
Hello,
we are working with TMS320LF2406A / 2407A processors and in the past we have used a TI utility named "f240_hex.exe" to convert .out files into .hex files. Those .hex files were then used for firmware updates via TI's Serial Flash Programming Utilities (SCI bootloader).
After migrating from Windows XP to Windows 7 (64-Bit), the f240_hex.exe utility now raises an error message due to Windows compatibility issues. The .hex file is not generated. Starting f240_hex.exe in XP compatibility mode doesn't solve the problem.
Is there a newer version or replacement for the f240_hex utility that also works under Windows 7, 64-Bit?
(I tried CodeComposer Studio's dsphex.exe, but couldn't get the same .hex format as before.)
Alternatively: Is there a document that describes the conversion algorithm of the f240_hex utility?
Any other ideas?
Any help would be appreciated,
Holger