This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Unexpected CCS graph wave

Hi,

I am testing HVPM_Sensored project on F28035 + PMSM hardware platform in real-time debug mode and observe qep1.ElecThet waveform through CCS , the graph is as shown in image1.png. The stable saw-tooth wave shape indicates the motor is  running smoothly. 

 

 However when I try to display  (_IQ(1.0) - qep1.ElecThet )  through the graph tool by the code:

DlogCh3 = (int16)_IQtoIQ15(_IQ(1.0) - qep1.ElecTheta);

I got a strange result as the wave shown in image2.png, that is sometimes I got a negative value( -1) from above calculation. This is quite hard to understand  as qep1.ElecThet falls in 0-1 and (_IQ(1.0) - qep1.ElecThet ) should also be in the range of 0-1.

What is wrong with it or is there  anything missed here? The version of ccs I am using is 4.2.2.