Other Parts Discussed in Thread: CONTROLSUITE
Dear All,
I'm testing my Concerto Based Development's Kit,
i started to develop some application with the only m3 CPU and so far, so good.
The second step has been to try developping an application for the C28 CPU.
I started by downloading and run the setup_m3.out on the M3 CPU, then, i built and downloaded an application on C28 CPU (let's say the cpu_timers example on the ControlSuite). The problem is that when i run the C28 executable, the debugger "jump" at the location <symbol is not available>0x3ff7ed.
I'm not very expert but in my opinion there could be some problem related to the .asm file linked to the application.
I using a CCS4.2.5, could the problem related to the CCS version?
Any comment will be appreciated.
Thanks
Andrea