Other Parts Discussed in Thread: TMS320F28035
Hello,
I'm trying to protect my program using the CSM feature from TMS320F28035 MCU.
After program the flash memory using the on chip flash programmer I change the code security password and program the password.
Finally I lock the code security password.
Up to this point, all is ok but the problem is that my program isn't working and I can't reconnect with the target.
When I try to connect I get this error:
=======================================================
Error connecting to the target:
Error 0x80002280/-1250
Fatal Error during: Target Communication, OCS, Control,
Device driver: Lost USB connection to emulator.
You should ABORT and restart to re-establish the USB link.
I/O Port = 510
Board Name: F28035
Cpu Name: TMS320F2800_0
=======================================================
Could someone tell me why I can't connect with the MCU again?