Other Parts Discussed in Thread: TMS320F28335, CONTROLSUITE
Last week I moved my CCS4 project to CCS5 because of the instability of CCS4 on Windows 7 x64. Debugging goes fine now, but I have a new (strange) prolem.
The same project with CCS5: 5.1.1.00031 with compiler TIv5.2.3 (Effective TI v6.0.2) builds with no errors (few warnings I think because of the migration).
Under CCS5: 5.2.0.00044 with compiler TI v5.2.3 (Effective TI v6.1.0.B1) there is an error with the cmd file: Cannot find file "Flash28335_API_V210.lib"
I can't find a solution for my problem, project properties seem the same, the files are from one repository.
The used device is a TMS320F28335, the lib file is placed in the "lib" folder in the project.