Hi All!
I have a brand new TMDSPREX28335: C2000 Peripheral Explorer Kit with code comoser studio Version: 5.1.0.09000 with Windows XP version 2002 Service Pack 3 . I first tried to connect it with USB connecter JP1 but every time target connection test failed. Then I tried it with JTAG Emulator X1B_1201378 which is compatable with XDS100v2. But I only could perform the target connection test as successful with XDS100v1 and Device Selected TMS320F28335. In docking station I have TMDSCNCD28335PFG CONTROL CARD.
My boot configration is as follows a jumper is placed at “J3”, and SW1 at TMDSCNCD28335PFG CONTROL CARD. is On plus SW2 have all 4 values OFF state
Every Time after compilation I get following errors
C28xx: Error connecting to the target: (Error -1135 @ 0x0) The emulator reported an error. Confirm emulator configuration and connections, reset the emulator, and retry the operation. (Emulation package 5.0.520.0)
or
C28xx: Error connecting to the target: (Error -1041 @ 0xFFFFFF87) The emulator reported an error. Confirm emulator configuration and connections, reset the emulator, and retry the operation. (Emulation package 5.0.520.0)
I am a student and working in a research institute . Any Help will be appritiated
Muhammad Ali