Hello. I try to use USER DEFINE TRAP (interrupt). What is the puprose of them and how can I use it? The only way that I have found is to call it from code like simple function. Is there any other option that this routine is call on event? What I need to do is when value of variable is for example 20000 then interrupt is generated by itself without any other conditions. So it needs to work asynchronously without extra conditionsin code, just with configuration.
Is that possible?
Thanks in advance
Piotr