This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Multiple ADCINT1 in vect table question



Hi,

I'm using the F28M35H52C1 and I'm using multiple ADCINTs.  I tried using ADCINT1, 2 in PIE Group 1 first and everyhting was fine as long as I used just those two. When I tried to use ADCINT3 as well I continually got the rsvd_ISR but  if I moved ADCINT1,2 into Group 10 and setup the Vector table in PieVect.h things worked as I expected.  Is it possible to use ADCINT1,2 in Group 1 and ADCINT3,4,5,6 in Group 10 or do they all need to be in Group 10 if using more than ADCINT1,2?

Its not an issue in my program since having all of them in Group 10 isn't a concern but I wanted to make sure that I was setting everything up correctly and wanted to verify the behavior.

Justin