This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

i'm looking for the best solution for using 7vdc bldc motor control

Other Parts Discussed in Thread: DRV8301, CONTROLSUITE, INSTASPIN-BLDC

Our motor spec : hall sensor BLDC motor

input voltage : 72VDC

Maximum Current : 100A

hi ..

i have to find solution for our motor contor.

we have 72vdc output battery and 72vdc input bldc motor.

i wanna make motor driver for our motor control.

if somebody know that.. the best solution for our motor control.

recommend please..

thank you.

  • unfortunately TI doesn't have a driver solution at that voltage level (support drivers for up to 60V like DRV8301)

    for control, I recommend looking at sensored BLDC through Piccolo controlSUITE (DRV8312-C2-KIT has an example) or look at sensorless InstaSPIN-BLDC