Hi!
I just installed the newest version of CCSv5 with the newest code generation tools for c2000 (6.1.0). Then I tried to compile a project (F28335) and got a lot of warnings because of the old flash api library I use. Hence, I immediately downloaded Control Suite and installed it. But the library file of the flash api is still version 2.10 and the same as in the year 2008. And the linker tells for each function I use:
warning: build attribute vendor section TI missing in
"../lib/Flash28335_API_V210/lib/Flash28335_API_V210.lib<Flash28_Erase.obj>":
compatibility cannot be determined
When will a new and compatible version be available? Until then I have to live with the warnings, or what can I do?
Best regards
Edwin Krasser