Hi,
Could anyone help me in putting together MPPT code for SEPIC based charger. Would be using F28069 exp kit.
Pl suggest.
thx & rgds
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Could anyone help me in putting together MPPT code for SEPIC based charger. Would be using F28069 exp kit.
Pl suggest.
thx & rgds
3443.SolarExplorer_PVBattChg_F2803x.zip
Attached is the software for the closed loop control of the sepic stage, it is based on F2803x however.
NOte: this is Beta minus version of the software
Paste it here
development_kits\SolarExplorer_v1.0 in controlsuite,
At this stage this is all i can help,
regards
Manish Bhardwaj
Dear Mr.Manish,
Thanks for the info. Its cool.
Could you pl share any documentation / instructions to run the code i.e., any incremental builds etc.
Could you please clarify which port should be connected to the power board?. The devinit_28035.c mentions PWM3 as spare
// GPIO-03 - PIN FUNCTION = --Spare--
GpioCtrlRegs.GPAMUX1.bit.GPIO3 = 1; // 0=GPIO, 1=EPWM2B, 2=SPISOMI-A, 3=COMP2OUT
// GpioCtrlRegs.GPADIR.bit.GPIO3 = 1; // 1=OUTput, 0=INput
Pl confirm my understanding..
Also pl suggest which declaration need to be defined for choosing mppt_incc and mppt_pno i.e, I would be using either of them and not both.
I suppose it could be ported to F28069 exp kit?. I could not get the DPLIB for 28069 from control suit?.
thx & rgds
Hello Mr Manish Bhardwaj,
I'm a Student and I'm working on the Solar explorer Development Kit with the Concerto Control Card. I want to use the Kit to charge a battery but it`s no program for this function in ControlSuite. Where can I find the Program for the Sepic Batt Charge for the Concerto F28M35H51C to drive the MPPT for the Sepic Stage.
Best regard,
Galeh
Hi,
have you instale Control suite. It`s a tool provides you informations and Documents about any Microcontroller of Texas Instrument.
You can also get there much example to simulate or to program you Kit.
Just tip "Control suite" in google search and you will find the new version from the web-site of Texas Instrument.
I you get any other problem you can send me a message.
Good luck.
Galeh
Thanks, another question. Do you know if the http://www.ti.com/tool/tmdssolarpexpkit
The secondary controller can run another algorithm like DC motor control
And can the PV emulator model feed power to the SEPIC stage of that controller?