Hi
I am trying to run blinked led project form flash. I have achieve from run but I can't from flash.
I applied steps in piccolo 1 day workshop. I load codes from flash. then debug codes. then run. Led blinked
then cpu reset. I clicked scripts,emu boot mode select,flash boot mode. then run, led blinked. Always ok. In that case I was able to load codes to flash.
then I terminate project and close code composer. I disconnect the ControlSTICK from the computer USB port. then re-connect the ControlSTICK to the computer USB port.
I hoped the LED should be blinking but led didnt blink.
what can I do?
According to piccolo 1 day workshop pdf when emulator not connected Boot determined by 2 GPIO pins and 2 OTP locations. What is these?
it says GPIO37 and 34 are used for boot determinde. but piccolo F28027 control stick dont have GPIO37. which ports for piccolo control stick ı must use?