Hi,
I've enabled the crystal operation and turned off other clock inputs (internal oscillators 1 and 2 and external oscillator) for F28035. According to the document sprugl8b.pdf (Figure 18: Clocking Options) it is possible to turn on just the crystal operation (with setting other bits correctly). But I've found that the internal oscillator 1 has to be turned on as well, although it is not used for any switch. Timer 2 is not used and it is configured per default (using SYSCLKOUT). This is the code:
Slavica