Other Parts Discussed in Thread: CONTROLSUITE
I'm trying to set up a new project for a F28035 and I am having problems with the linker files.
I been trying to get the same set up as the examples, with F28035_FLASH.CMD, F28035_RAM.cmd and DSP2803x_Headers_nonBIOS.cmd obviously Flash and Ram depend on the build configuration and are excluded automatically depending which configuration is selected. Even if I set the linker file on a per configuration basis in the project properties both files are shown as active regardless of the build configuration. Also manually adding the nonBIOS file results in it being excluded from the build.
Can anyone point me in the right direction?
Using CCSv5.2.0.00069
Thanks
Steve