I'm facing some connection problems between emulator XDS100v2 and MCU Concerto F28M35H52C1.
I installed CCSv5 and the latest Control Suite version. Using integrated emulator of Concerto Control Card, connected to USB J20, everything seems to work correctly.
If i try to use an external XDS100v2 connected to JTAG 14 pin connector (J2) of docking station, I obtain this message:
"IcePick_C_0: Error connecting to the target: (Error -2131 @ 0x0) Unable to access device register. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 5.0.501.0)"
Before that, I mounted zero Ohm resistors on R40..R46 and closed jumper J8 to inhibit docking station xds100.
That's all I've done. Have I need to do some more settings to use an external xds100v2 with concerto control cards?
Thanks in advance.