This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Question on application report SPRAAM3

Where can I get the code associated with this app report:

http://www.ti.com/mcu/docs/litabsmultiplefilelist.tsp?sectionId=96&tabId=1502&literatureNumber=spraam3&docCategoryId=1&familyId=1523

Is the board available for purchased from TI?

If not, I need to get a motor control board based on the 2808, any recommendation?

Thanks.

  • TuanHo,

    I know that this board is not available for purchase.  I took a quick look and I do not believe the software is available either.

    If you are not concerned with writing some code, one idea may be to purchase the TMDS2MTRPFCKIT and the TMDSCNCD2808.  The F2808 controlCARD will be able to work with the DRV8412-C2-KIT, but the software that comes with the kit will be for the F28035.

    Is there any particular particular reason you are interested in the F2808?  If not, the DRV8412-C2-KIT (built around the F28035) sounds like a kit that has very similar features to the one you've mentioned.


    Thank you,
    Brett

  • We have a board design using the 2808 so I'd like to keep it the same.

    I need an EVM that can drive low voltage brushed DC motor with encoder feedback and I'm having a hard time finding one.

    Thanks.

  • TuanHo,

    After asking around, I don't think we have a board like you are wanting. 

    Note that it is possible to do brushed control with the F2808 though.


    Thank you,
    Brett