Other Parts Discussed in Thread: TMS320F28335
Hi folks,
I an trying to activate two ISRs in my code, one for ePwm and the other for ADC.
However, I can only have "IER |= 1" to activate the interrupt for ADC or "IER |=4" to do the same for ePwm.
Is there any way to temporarily change the IER value inside the ISRs? I tried it but it failed!
By the way, I noticed that the priority of the ADC interrupt is higher that that of the ADC.
Thanks
Ali