Hi there,
I've purchased the dual axis low voltage motor control kit. I've read the documentation and am trying out the examples provided. I established the following:
- The motors are pmsm.
- The Space Vector control examples are based on sensorless control.
- In the examples, sensored SV control is achieved using Quadrature encoders.
- The motors come with hall sensors, not QE.
- Hall sensors (in the examples) are used only for trapezoidal control of BLDC Motors.
I'd like to achieve sensor based SV control using the motors provided......
Will I have to convert my hall sensor signals into QEP signals?
Kind regards
Sjerra