Other Parts Discussed in Thread: CONTROLSUITE
Hi all,
We are developing a secondary bootloader for the Piccolo device, TMS32F28023. It is intended to be use as a FLASH programmer
1) the DSP is first entered in SCIBOOT mode by pulling TDO (GPIO37) low
2) Transfer the secondary bootloader to the RAM by using the bootrom in SCI boot mode
3) Transfer the application code & burn into DSP flash, by using the secondary boot loader.
The secondary bootloader is very similar to the CFKA module in http://www.ti.com/lit/an/spraaq2/spraaq2.pdf ; and it will be used in a production line for fresh DSP, which are not programmed at all.
My issues with the secondary bootloader is that it does NOT boot up after step 2) above. The Sciboot bootrom in the DSP accepts & echoes back every bytes that sent through the console via serial, but it seems to be stuck after secondary boot loader data transferred -- Doesn't seem to be able to branch to the secondary bootloader just transferred. If I use JTAG immediately without power off, I can see the contents in the RAM is the same as the transferred file; and if I set the PC (porgram counter) to 0 , which is the entry point of the secondary bootloader and hit run, then the secondary bootloader runs as expected... This makes me to think that although the secondary boot is transferred correctly via serial, the SCIBOOT bootrom stucks somewhere after file tansfer...
I've been reading a few notes on Piccolo bootloader, but most of them are flash based ... This RAM based secondray bootloader is quite rare.
Regards,
XIng