This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UART Problem with Delfino Exp.Kit TMSC28346

Hello,

I'm working with Delfino DIM168 Exp.Kit C28346 and with SIMULINK (Embedded Coder).

Everything works fine (ePWM, eQEP) but now i would like to send commands with HTerm(Hyperterminal Software) to the Target.

So i tick the VCP box in the Hardware Preferences. Virtual Port COM4 appears in Hardware Preferences and in HTerm.

After compiling I can't Connect to COM4.

Error: COM4 is blocked.

I hope you can help me.

MATLAB Version 7.13.0.564 (R2011b)

Code Composer Version: CCSv3.3 (XDS100v1)

[C2834x needs XDS100v2 but is not supported for CCSv3.3 is that right? Is there a Problem ? The other peripherals work fine with Simulink !]

Best Regards

Dennis