Other Parts Discussed in Thread: TMS320F28035
hello :
somebody can help me a strange problem that occurred on the need to hard reset to work properly.
1.When failures occur, the motor can not automatically enter the closed-loop control.
2.Press the "restart button" to restart the operation of the motor is still invalid in CCSV4.2 version
DEBUG mode.
3.After each failure as long as the debug mode, press the reset button and then press the play button
will be able to immediately make the motor smooth entry into the closed-loop control.
4.Hundred times per normal operation there will be a failure. (TMS320F28035 HVPM_Sensorless)
5.RESET and RESTART function key difference allows the programs have different execution results?
THANKS.
Dowsheng.