Hello, I'm an engineer from Novosibirsk. I examine the work of PLC in an example of TMDSPLCKIT-V3. I have a problem with programming TMS320F28069. It is my first time working with DSPBIOS. I can't find a driver for the UART. In the example of the package ControlSUITE (DSP280x_examples_ccsv4) UART is implemented through surveys of the flags (SciaRegs.SCIFFTX.bit.TXFFST and SciaRegs.SCIFFRX.bit.RXFFST) what is unacceptable in my project. Included with the KIT library is uart_f2806x.lib, but there is no description of it and even a *.h file. Will be great, if You give me a sample working DSPBIOS UART project for CCS .