Hi,
Can anyone favourably tell me what is the maximum clock frequency achievable using the on-chip Osc of the F28069?
Thank you.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Highest supported SYSCLK for this device is 90 MHz. You can achieve this using the PLL to do x18/2 or x9/1 of the 10 MHz internal oscillator.
Kris