Hi,
I am using HV_SOLAR_DC_AC development kit. I don't have DC-DC solar boost converter so I am using DC supply at the input.
Everything works fine in the Open Loop Build without PLL and with PLL. But when I connect to the grid, my DC Bus starts to rise when the relays opened and the device goes to DC bus over voltage error. I installed the C1 bulk capacitor (1 mF, 350V) and I am using a DC supply of 300 volts. My grid is 230Vac, and I changed the grid settings accordingly..
Somehow it seems the inverter works as a boost converter?
Thanks,
Celil