I'm using the example code for a F28027 and am trying to check the PLL is set properly through Flash_ToggleTest() in the Flash API. It is always 1.25MHz instead of the required 10kHz.
My code is just basic and is loaded through SCI_Boot. I use GPIO32 to read the output. The functions being called are the ones provided by the examples (DSP2802x_SysCtrl.c, etc). There is 18.432MHz between X1 & X2, but INTOSC1 is being used. I get 60MHz on XCLKOUT.
If anybody has any ideas why this could not be working, I would love to hear them! The code is below.
void main(void)
{
// PLL, WatchDog, enable Peripheral Clocks
InitSysCtrl();
// Disable CPU interrupts
DINT;
// The default state is all PIE interrupts disabled and flags are cleared
InitPieCtrl();
// Disable CPU interrupts and clear all CPU interrupt flags:
IER = 0x0000;
IFR = 0x0000;
// Initialize the PIE vector table with pointers to the shell Interrupt
// Service Routines (ISR).
InitPieVectTable();
// Init flash
InitFlash();
Flash_CPUScaleFactor = SCALE_FACTOR;
Flash_CallbackPtr = 0;
EALLOW;
GpioCtrlRegs.GPBMUX1.all = 0;
GpioCtrlRegs.GPBDIR.all = 0x00000001;
EDIS;
Flash_ToggleTest(&GpioDataRegs.GPBTOGGLE.all, 0x00000001);
}