This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Windoes Application (C# & visula Studio) to get the A/D channels



Hello:

I have a eZdsp-2407 eval board from spectrum and wrote an application that outputs 7 A/D channels thru the serial port to a PC (CSV format) and then using Excel I plot the data for all the capture channels. 

I would like to plot the same data for each of the A/D channels on the piccolo or concerto experimenter board.

Do you ave any sample code to do this with the piccolo or the concerto? 

Is there an application written in C# (or other language for visual studio) that will allow me to get and plot the A/D channels real time (or store the data), instead of using excel?

Thank you

Julio