Other Parts Discussed in Thread: TMS320F28035
hello,
I've got some problems with the following kit:
TMS320C2000
TMDSHVMTRPFCKIT 28035 Piccolo-ControlCard
I went step by step through the "How to run" and "HW" guide.
My settings:
J3,J4,J5 [all main] are populated J5[M3] is not.
J2[main] is connected between the "Bridge" and the middle pin.
BS1 and BS5 are also connected via banana-plug.
(a) J9 is not populated due to the fact, that the DIMM-Card(28035) is in J1.
This confuses me, because the "HW" guide says, that:
'[Main] J9
JTAG TRSTn disconnect jumper, populating the jumper enables JTAG
connection to the microcontroller. The jumpers needs to be unpopulated
when no JTAG connection is required such as when booting from FLASH.'
But this would be the complete opposite of (a) and I have to poulate J9 for programming the controller on the Piccolo ControlCard.
despite that I need the xds100 Emulator and therefore the JTAG all the time to work with the kit via the pc.
Is that right (referring to the J9-topic)?
The cable for the USB JTAG (XDS-100)Emulator is plugged in the usb port on the pc and the kit. (LD1 is on)
I connected the DC power entry [M6] (and also tried without it, thinking that the supply from the pc-usb should be enough.)
With the DC power, I think a pre-flashed program is instantly running and turns the fan for cooling the inverter on maximum speed.
In order to stop it and change running programs I have to connect the kit.
My settings for the target configuartion in CCS:
'Texas Instruments XDS100v1 USB Emulator
TMS320F28035'
CCS version: 4.2.3.00004
There seems to be a connection problem. I receive the following statements during debugging (it is one of the ti sample
programs 'HVMotorCtrl+PfcKit_v2.0'):
marginal note:
After importing existing project from the controlsuit I get an Error: (see below)
(For half the projects)
I couldn't rebuild the other successful imported half of the projects. It only works after installing a newer code generator version, but I have to do it manually.
(The update function in CCS creates only an empty folder.)
I still don't really know what exactly to do to get all the examples working.
My CGT version is now:TI v6.0.1.
After starting debug, the console opens with 'Error 1135' (see below)
Then I reseted the emulator and debug it again. This time 'Error 1041' shows up.
The device manager shows:
-XDS-560 JTAG Emulator (with warning sign, but it seems to be irrelevant)
-a new COM Port appears
-TI XDS100 Channel A
-TI XDS100 Channel B
I've checked the eeprom programming; the values are:
VID:0403
PID:A6D0
Everything seems to be ok, concerning the hardware connections.
What power supply is exactly necessary to run and program the Controller on the Card?
(At the moment I don't want to connect the kit to a motor, so it's all about programming.)
Are my mentioned hardware-settings ok?
Or is there a complete other problem I'm missing?
best regards and thanks