Hi. im working with the F28335 on a Photovoltaic application
im using the ADC to sense voltage and current and PWM to control the Duty ratio
now im changing the duty ratio and it seems that in some point my DSP fails and disconnects from the CCS and i have to close all and start again.
i think that is because when i change the duty ratio i get many spikes in my voltage signal and i see that this spikes reach negative values and might reach more than 3 volts on the ADC
would this affect to the performance of the ADC and the DSP? how can i make it ignore this noise from the sensors (if that is the case)