This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Issue with CAN transmit and receive pgms.. Pls help...

Hi ,

       I am trying to transmit a message from a TMS320F28069 experimental kit to another one of the same kind. I have tried ecanback2back  pgm without STM mode and could successfully see the signals getting transmitted on the can lines.

1.I have written a code for transmission on one dsp and that for reception at the other. The 230QD transceiver is used. There are 120 ohm resistors connected at the 2 ends of a shielded cable which connects the 2 DSPs. I am sensing the voltage through ADC2 and is voltage there exceeds 1.5V, I need to send messages through CAN.I am sending messages through mailbox5 only. I can see the message(CANMDL and CANMDH contents) sent on the watch window.But there is  no signal across the CAN lines. Can someone help me on this?

2. The BRPreg value given in ecanback2back eg is 1 which corresponds to 40MHz operation. Won't this value be too high for CAN to operate when I am trying to transmit data to another node? I also tried with BRPreg = 19. But I did not get any signal on the line.

3. When the receive pgm gets executed, the CANRMP doesnot get set to 0xFFFFFFFF. Hence it goes into an infinite loop. I tried to force CANRMP to be equal to 0xFFFFFFFF in the pgm but it remains at 0x00000000. Also, the can mailbox contents show some erronoeus values.

I am pasting both the codes here. Pls help me urgently as I have a very tight deadline.

#include "PeripheralHeaderIncludes.h"
#include "F2806x_EPwm_defines.h"        // useful defines for initialization
#include "DSP28x_Project.h"     // Device Headerfile and Examples Include File

//%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%
// FUNCTION PROTOTYPES
//%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%

void DeviceInit(void);
void InitFlash();
void MemCopy(Uint16 *SourceAddr, Uint16* SourceEndAddr, Uint16* DestAddr);

//%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%
// VARIABLE DECLARATIONS - GENERAL
//%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%%

// Used for running BackGround in flash, and ISR in RAM
extern Uint16 RamfuncsLoadStart, RamfuncsLoadEnd, RamfuncsRunStart;



Uint16 LoopCount=0;
Uint16 i,endcount=0;
Uint16 j,count=0;
Uint32  temp,ErrorCount=0;//ecan
Uint16 Voltage_ADC2;
float duty_cycle_A = 1666;
Uint16 duty_cycle_B=2000;

void main(void)
{
    Uint16 i = 0;
    struct ECAN_REGS ECanaShadow;
      DeviceInit();    
#ifdef FLASH        
    MemCopy(&RamfuncsLoadStart, &RamfuncsLoadEnd, &RamfuncsRunStart);
    InitFlash();    // Call the flash wrapper init function
#endif //(FLASH)
    DINT;
    IER = 0x0000;
   IFR = 0x0000;
    EALLOW;
       AdcRegs.ADCCTL1.bit.ADCBGPWD    = 1;    // Power up band gap
       AdcRegs.ADCCTL1.bit.ADCREFPWD    = 1;    // Power up reference
       AdcRegs.ADCCTL1.bit.ADCPWDN     = 1;    // Power up rest of ADC
    AdcRegs.ADCCTL1.bit.ADCENABLE    = 1;    // set timming to 13cycles as required by ADC module
    for(i=0; i<5000; i++){}                    // wait 60000 cycles = 1ms (each iteration is 12 cycles)
    AdcRegs.ADCCTL1.bit.INTPULSEPOS    = 1;    // create int pulses 1 cycle prior to output latch
    AdcRegs.ADCSOC0CTL.bit.CHSEL     = 2;    //set SOC0 channel select to ADCINA2
    AdcRegs.ADCSOC0CTL.bit.TRIGSEL     = 5;    //set SOC0 start trigger on EPWM1A, due to round-robin SOC0 converts first then SOC1
    AdcRegs.ADCSOC0CTL.bit.ACQPS     = 8;    //set SOC0 S/H Window to 8 ADC Clock Cycles, (8 ACQPS plus 1)
    EDIS;

   EPwm1Regs.ETSEL.bit.SOCAEN    = 1;        // Enable SOC on A group
   EPwm1Regs.ETSEL.bit.SOCASEL    = 4;        // Select SOC from from CPMA on upcount
   EPwm1Regs.ETPS.bit.SOCAPRD     = 1;        // Generate pulse on 1st event
   EPwm1Regs.CMPA.half.CMPA     = 500;        // Set compare A value, duty cycle 50% initially
   EPwm1Regs.TBPRD                 = 1000;        // Set period, 80kHz when PLL is set to 0x10 (80MHz)
   EPwm1Regs.TBCTL.bit.CTRMODE     = 0;        // count up and start
       EPwm1Regs.TBPHS.all = 0;                   // Time-Base Phase Register
       EPwm1Regs.TBCTR = 0;                       // Time-Base Counter Register    
        EPwm1Regs.TBCTL.bit.PRDLD = TB_IMMEDIATE;  // Set Immediate load
        EPwm1Regs.TBCTL.bit.PHSEN = TB_DISABLE;       // Disable phase loading
    EPwm1Regs.TBCTL.bit.SYNCOSEL = TB_SYNC_DISABLE;
    EPwm1Regs.TBCTL.bit.HSPCLKDIV = TB_DIV1;
    EPwm1Regs.TBCTL.bit.CLKDIV = TB_DIV1;
        EPwm1Regs.TBCTL.bit.CTRMODE = TB_COUNT_UP; // Count-up mode: used for asymmetric PWM
       EPwm1Regs.CMPCTL.bit.SHDWAMODE = CC_SHADOW;
       EPwm1Regs.CMPCTL.bit.LOADAMODE = CC_CTR_ZERO;    // load on CTR=Zero
         EPwm1Regs.AQCTLA.bit.ZRO = AQ_SET;            // Set PWM2A on Zero
       EPwm1Regs.AQCTLA.bit.CAU = AQ_CLEAR;          // Clear PWM2A on event A, up count
    EALLOW;
    GpioCtrlRegs.GPAPUD.bit.GPIO30 = 0;     // Enable pull-up for GPIO30 (CANRXA)
        GpioCtrlRegs.GPAPUD.bit.GPIO31 = 0;     // Enable pull-up for GPIO31 (CANTXA)
        GpioCtrlRegs.GPADIR.bit.GPIO30 = 0;
        GpioCtrlRegs.GPADIR.bit.GPIO31 = 1;
        GpioCtrlRegs.GPAQSEL2.bit.GPIO30 = 3;
        GpioCtrlRegs.GPAMUX2.bit.GPIO30 = 1;    // Configure GPIO30 for CANRXA operation
        GpioCtrlRegs.GPAMUX2.bit.GPIO31 = 1;    // Configure GPIO31 for CANTXA operation
        EDIS;
         for(;;)  //infinite loop
        {
        LoopCount++;
            Voltage_ADC2 = AdcResult.ADCRESULT0;    //add Voltage_ADC2 to watch window
            voltage = (AdcResult.ADCRESULT0*3.3)/4095;
             if(voltage>1.5)
             {
                 EALLOW;
                 ECanaShadow.CANTIOC.all = ECanaRegs.CANTIOC.all;
                 ECanaShadow.CANTIOC.bit.TXFUNC = 1;
                 ECanaRegs.CANTIOC.all = ECanaShadow.CANTIOC.all;
                ECanaShadow.CANMC.all = ECanaRegs.CANMC.all;
                ECanaShadow.CANMC.bit.SCB = 1;
                ECanaRegs.CANMC.all = ECanaShadow.CANMC.all;
                ECanaMboxes.MBOX0.MSGCTRL.all = 0x00000000;
                ECanaMboxes.MBOX1.MSGCTRL.all = 0x00000000;
                ECanaMboxes.MBOX2.MSGCTRL.all = 0x00000000;
                ECanaMboxes.MBOX3.MSGCTRL.all = 0x00000000;
                ECanaMboxes.MBOX4.MSGCTRL.all = 0x00000000;
                ECanaMboxes.MBOX5.MSGCTRL.all = 0x00000000;
                ECanaMboxes.MBOX6.MSGCTRL.all = 0x00000000;
                ECanaMboxes.MBOX7.MSGCTRL.all = 0x00000000;
                ECanaMboxes.MBOX8.MSGCTRL.all = 0x00000000;
                ECanaMboxes.MBOX9.MSGCTRL.all = 0x00000000;
                ECanaMboxes.MBOX10.MSGCTRL.all = 0x00000000;
                ECanaMboxes.MBOX11.MSGCTRL.all = 0x00000000;
                ECanaMboxes.MBOX12.MSGCTRL.all = 0x00000000;
                ECanaMboxes.MBOX13.MSGCTRL.all = 0x00000000;
                ECanaMboxes.MBOX14.MSGCTRL.all = 0x00000000;
                ECanaMboxes.MBOX15.MSGCTRL.all = 0x00000000;
                ECanaMboxes.MBOX16.MSGCTRL.all = 0x00000000;
                ECanaMboxes.MBOX17.MSGCTRL.all = 0x00000000;
                ECanaMboxes.MBOX18.MSGCTRL.all = 0x00000000;
                ECanaMboxes.MBOX19.MSGCTRL.all = 0x00000000;
                ECanaMboxes.MBOX20.MSGCTRL.all = 0x00000000;
                ECanaMboxes.MBOX21.MSGCTRL.all = 0x00000000;
                ECanaMboxes.MBOX22.MSGCTRL.all = 0x00000000;
                ECanaMboxes.MBOX23.MSGCTRL.all = 0x00000000;
                ECanaMboxes.MBOX24.MSGCTRL.all = 0x00000000;
                ECanaMboxes.MBOX25.MSGCTRL.all = 0x00000000;
                ECanaMboxes.MBOX26.MSGCTRL.all = 0x00000000;
                ECanaMboxes.MBOX27.MSGCTRL.all = 0x00000000;
                ECanaMboxes.MBOX28.MSGCTRL.all = 0x00000000;
                ECanaMboxes.MBOX29.MSGCTRL.all = 0x00000000;
                ECanaMboxes.MBOX30.MSGCTRL.all = 0x00000000;
                ECanaMboxes.MBOX31.MSGCTRL.all = 0x00000000;
                ECanaRegs.CANTA.all = 0xFFFFFFFF;   /* Clear all TAn bits */
    ECanaRegs.CANRMP.all = 0xFFFFFFFF;  /* Clear all RMPn bits */
    ECanaRegs.CANGIF0.all = 0xFFFFFFFF; /* Clear all interrupt flag bits */
    ECanaRegs.CANGIF1.all = 0xFFFFFFFF;
    ECanaShadow.CANMC.all = ECanaRegs.CANMC.all;
    ECanaShadow.CANMC.bit.CCR = 1 ;            // Set CCR = 1
    ECanaRegs.CANMC.all = ECanaShadow.CANMC.all;
       do
    {
      ECanaShadow.CANES.all = ECanaRegs.CANES.all;
    } while(ECanaShadow.CANES.bit.CCE != 1 );       // Wait for CCE bit to be set..
    ECanaShadow.CANBTC.all = 0;
    ECanaShadow.CANBTC.bit.BRPREG = 1;
    ECanaShadow.CANBTC.bit.TSEG2REG = 4;
    ECanaShadow.CANBTC.bit.TSEG1REG = 13;
    ECanaShadow.CANBTC.bit.SAM = 1;
    ECanaRegs.CANBTC.all = ECanaShadow.CANBTC.all;
    ECanaShadow.CANMC.all = ECanaRegs.CANMC.all;
    ECanaShadow.CANMC.bit.CCR = 0 ;            // Set CCR = 0
    ECanaRegs.CANMC.all = ECanaShadow.CANMC.all;
     do
    {
      ECanaShadow.CANES.all = ECanaRegs.CANES.all;
    } while(ECanaShadow.CANES.bit.CCE != 0 );       // Wait for CCE bit to be  cleared..
    ECanaRegs.CANME.all = 0;        // Required before writing the MSGIDs
    EDIS;
    ECanaMboxes.MBOX5.MSGID.all = 0x00140000; // Std identifier
     ECanaRegs.CANME.all = 0xFFFFFFFF;
     ECanaMboxes.MBOX5.MSGCTRL.bit.DLC = 8;
     EALLOW;
    ECanaShadow.CANMD.all = ECanaRegs.CANMD.all;
    ECanaShadow.CANMD.bit.MD5 = 0;
    ECanaRegs.CANMD.all = ECanaShadow.CANMD.all;
     ECanaMboxes.MBOX5.MSGCTRL.bit.DLC = 8;
     ECanaMboxes.MBOX5.MDL.all = 0x00140000;
     ECanaMboxes.MBOX5.MDH.all = 0x89ABCDEF;
    ECanaRegs.CANMIM.all = 0xFFFFFFFF;
     ECanaShadow.CANMC.all = ECanaRegs.CANMC.all;
   ECanaShadow.CANMC.bit.STM = 0;    // Configure CAN for self-test mode
   ECanaRegs.CANMC.all = ECanaShadow.CANMC.all;
    EDIS;
    ECanaRegs.CANTRS.all = 0x00000020;
    while(ECanaRegs.CANTA.all == 0x00000020){}// for maibox 5 only
    ECanaRegs.CANTA.all == 0x00000020;
    endcount++;
    }
    else
    {
        temp++;
    }
  }
}

The receive code on the second DSP is as follows

#include "PeripheralHeaderIncludes.h"
#include "F2806x_EPwm_defines.h"         // useful defines for initialization
#include "DSP28x_Project.h"
 
void DeviceInit(void);
void InitFlash();
void MemCopy(Uint16 *SourceAddr, Uint16* SourceEndAddr, Uint16* DestAddr);
void mailbox_check(int32 T1, int32 T2, int32 T3);
void mailbox_read(int16 i);
extern Uint16 RamfuncsLoadStart, RamfuncsLoadEnd, RamfuncsRunStart;
Uint16 LoopCount,i,j,temp=0;

Uint32  ErrorCount;
Uint32  PassCount;
Uint32  MessageReceivedCount;
Uint32 RXCOUNT;
Uint32  TestMbox1 = 0;
Uint32  TestMbox2 = 0;
Uint32  TestMbox3 = 0;

void main()
{
    
struct ECAN_REGS ECanaShadow;
DeviceInit();
    EALLOW;
    ECanaShadow.CANRIOC.all = ECanaRegs.CANRIOC.all;
    ECanaShadow.CANRIOC.bit.RXFUNC = 1;
    ECanaRegs.CANRIOC.all = ECanaShadow.CANRIOC.all;

    ECanaShadow.CANMC.all = ECanaRegs.CANMC.all;
    ECanaShadow.CANMC.bit.SCB = 1;
    ECanaRegs.CANMC.all = ECanaShadow.CANMC.all;
      
    ECanaRegs.CANRMP.all = 0xFFFFFFFF;  /* Clear all RMPn bits */
    ECanaRegs.CANGIF0.all = 0xFFFFFFFF; /* Clear all interrupt flag bits */
    ECanaRegs.CANGIF1.all = 0xFFFFFFFF;
    ECanaShadow.CANMC.all = ECanaRegs.CANMC.all;
    ECanaShadow.CANMC.bit.CCR = 1 ;            // Set CCR = 1
    ECanaRegs.CANMC.all = ECanaShadow.CANMC.all;
    do
    {
      ECanaShadow.CANES.all = ECanaRegs.CANES.all;
    }while(ECanaShadow.CANES.bit.CCE == 0);      // Wait for CCE bit to be set..

    ECanaShadow.CANBTC.all = 0;
    ECanaShadow.CANBTC.bit.BRPREG = 1;
    ECanaShadow.CANBTC.bit.TSEG2REG = 4;
    ECanaShadow.CANBTC.bit.TSEG1REG = 13;
    ECanaShadow.CANBTC.bit.SAM = 1;
    ECanaRegs.CANBTC.all = ECanaShadow.CANBTC.all;
    ECanaShadow.CANMC.all = ECanaRegs.CANMC.all;
    ECanaShadow.CANMC.bit.CCR = 0 ;            // Set CCR = 0
    ECanaRegs.CANMC.all = ECanaShadow.CANMC.all;
    ECanaRegs.CANME.all = 0;        // Required before writing the MSGIDs
    EDIS;
     ECanaMboxes.MBOX1.MSGID.all  = 0x00040000;  // Std identifier
    ECanaMboxes.MBOX2.MSGID.all  = 0x00080000;  // Std identifier
    ECanaMboxes.MBOX3.MSGID.all  = 0x000C0000;  // Std identifier
    ECanaMboxes.MBOX4.MSGID.all  = 0x00100000;  // Std identifier
    ECanaMboxes.MBOX5.MSGID.all  = 0x00140000;  // Std identifier
    ECanaMboxes.MBOX6.MSGID.all  = 0x00180000;  // Std identifier
    ECanaMboxes.MBOX7.MSGID.all  = 0x001C0000;  // Std identifier
    ECanaMboxes.MBOX8.MSGID.all  = 0x00200000;  // Std identifier
    ECanaMboxes.MBOX9.MSGID.all  = 0x00240000;  // Std identifier
    ECanaMboxes.MBOX10.MSGID.all = 0x00400000;  // Std identifier
    ECanaMboxes.MBOX11.MSGID.all = 0x00440000;  // Std identifier
    ECanaMboxes.MBOX12.MSGID.all = 0x00480000;  // Std identifier
    ECanaMboxes.MBOX13.MSGID.all = 0x004C0000;  // Std identifier
    ECanaMboxes.MBOX14.MSGID.all = 0x00500000;  // Std identifier
    ECanaMboxes.MBOX15.MSGID.all = 0x00540000;  // Std identifier
    ECanaMboxes.MBOX16.MSGID.all = 0x00580000;  // Std identifier
    ECanaMboxes.MBOX17.MSGID.all = 0x005C0000;  // Std identifier
    ECanaMboxes.MBOX18.MSGID.all = 0x00600000;  // Std identifier
    ECanaMboxes.MBOX19.MSGID.all = 0x00640000;  // Std identifier
    ECanaMboxes.MBOX20.MSGID.all = 0x00800000;  // Std identifier
    ECanaMboxes.MBOX21.MSGID.all = 0x00840000;  // Std identifier
    ECanaMboxes.MBOX22.MSGID.all = 0x00880000;  // Std identifier
    ECanaMboxes.MBOX23.MSGID.all = 0x008C0000;  // Std identifier
    ECanaMboxes.MBOX24.MSGID.all = 0x00900000;  // Std identifier
    ECanaMboxes.MBOX25.MSGID.all = 0x00940000;  // Std identifier
    ECanaMboxes.MBOX26.MSGID.all = 0x00980000;  // Std identifier
    ECanaMboxes.MBOX27.MSGID.all = 0x009C0000;  // Std identifier
    ECanaMboxes.MBOX28.MSGID.all = 0x00A00000;  // Std identifier
    ECanaMboxes.MBOX29.MSGID.all = 0x00A40000;  // Std identifier
    ECanaMboxes.MBOX30.MSGID.all = 0x00C00000;  // Std identifier
    ECanaMboxes.MBOX31.MSGID.all = 0x00C40000;  // Std identifier
    ECanaMboxes.MBOX0.MSGID.all =  0x00C80000;  // Std identifier
    ECanaShadow.CANMD.all = ECanaRegs.CANMD.all;
    ECanaShadow.CANMD.all = 0xFFFFFFFF;
    ECanaRegs.CANMD.all = ECanaShadow.CANMD.all; 
    ECanaShadow.CANME.all = ECanaRegs.CANME.all;
    ECanaShadow.CANME.all = 0xFFFFFFFF;
    ECanaRegs.CANME.all = ECanaShadow.CANME.all; 
    while(1)
    {
   while(ECanaRegs.CANRMP.all != 0x00000020 ) {}  // Wait for all RMPn to be set..
                
     ECanaRegs.CANRMP.all = 0x00000020;   // Clear all RMPn bits and start
     RXCOUNT++ ;  
     for(j=1; j<32; j++)         // Read & check 16 mailboxes
       {
          mailbox_read(j);         // This func reads the indicated mailbox data
          mailbox_check(TestMbox1,TestMbox2,TestMbox3); // Checks the received data
       }                         // all over again...
    }   
}
void mailbox_read(int16 MBXnbr)
{
   volatile struct MBOX *Mailbox;
   Mailbox = &ECanaMboxes.MBOX0 + MBXnbr;
   TestMbox1 = Mailbox->MDL.all;
   TestMbox2 = Mailbox->MDH.all;
   TestMbox3 = Mailbox->MSGID.all;


void mailbox_check(int32 T1, int32 T2, int32 T3)
{
    if((T1 != T3) || ( T2 != 0x89ABCDEF))
    {
       ErrorCount++;
    }
    else
    {
       PassCount++;
    }
}

------------------------------------------------------------------------------------------------------------------------------------------

The RXCOUNT is getting incremented when the while loop shown above is commented ; but CANRMP is always 0x00000000.

Pls help!

Keerthi