This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV8301 EVM Board

Can I use the DRV8301-HC-EVM Board with a F28069 DIMM ControlCARD instead of the provided CC2803X ISO DIMM card?  Besides the processor, it looks like the main difference between the two is the on-board isolated JTAG interface. I have a Blackhawk USB560M JTAG Emulator, can I use it on J21 on the DRV8301-HC-EVM Board?