This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

f28069 power supply pins



I am working on a board based on f28069 (F28069U-PZPS), just one clarification about the power supply pins. One reference schematic shows each pin connected through inductors (BKP2125HS600-T) from a common supply. Can I simply connect them directly from a digital 3.3V? I am planning to add an inductor to separate analog and digital supplies. What is the advantage of connecting so many inductors? Or what could be the effect if I tie all pins (5,13,38..) together to a digital 3.3V supply?

Thanks in advance

Joy