Other Parts Discussed in Thread: TMS320F28069
Hi,
I want to connect with the uC only via USB. But first, i have to Enable the USBIOEN bit in the GPACTRL2 Register. I dont know how to communicate with the uC to set the
suitable bit when the USB Controller is still disabled. Is it possible to enable the usb by a Pin, or do i have to connect with an other communication bus like Can?
Or did i just get it wrong and i can connect to the controller without any changes?
Im using the tms320F28069 (100Pin).
Thanks!