Other Parts Discussed in Thread: CONTROLSUITE
I need help with compiler error. I tried to add the UARTstdio library to my project, which is based off the example project "Example_2806xCpuTimer", so that i can use the UARTprintf function. I'm using the F28069 USB dev board with ccs5.
Here's what I did.
1. Went into project -> properties, add this include directory under c2000 compiler include options: "${INSTALLROOT_F2806x_V130_TO_MWARE}"
2. Add this line to top of my Example_2806xCpuTimer.c: #include "utils/uartstdio.h"
3. Called printf function: UARTprintf("hello\r\n");
4. Compiled, got these two errors: "errors encountered during linking; "Example_2806xCpuTimer.out" not built" and "unresolved symbols remain"
Any idea what I messed up?
Library located here: C:\ti\controlSUITE\device_support\f2806x\v130\MWare\utils
Thanks,
Jut