Hello,
I'm working with eZdsp F28335 Controller and with Matlab Simulink (IDE CCSv3.3)
I have an extern signal source (5kHz PWM) and would synchronize the ePWM Moduls on two diffrent F28335 Controller.
Is this possible ?
On the ePWM Moduls I tick the "Add S/W sync input port" (Input port appears).
Than I connect the GPIO(20) Input (external PWM) with the Sync Input port of the ePWM in my Model.
After that i run the Programm on two diffrent F28335 DSP and connect the external PWM on GPIO(20).
But if i display the two PWM Signal on an oscilloscope the two PWM would be phase shifted.
Please help me.
Best Regards
Dennis